Other Parts Discussed in Thread: LM2611, LM5001
Dear Team,
Do you have suitable for 12V==>-12V device?
Or reference design?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin
I would suggest a flyback solution using a device LM5001. to generate 5V 0.4A as in datasheet page 15, figure 19. then a LDO or buck to generate the 3.3V 0.3A from the 5V output.