Other Parts Discussed in Thread: TPS2420, TPS2590, TPS25982
Hi team,
My customer is evaluating the TPS259531 in the USB Vbus over-current protection function. They tested our EVM and set the current limit to 2A. As TPS2595 will disconnect the load based on the detection of device temperature, customer thought the time is too long from over-current event happening to disconnecting the load. So I just want to check with you do we have any other E-fuse solution can immediately disconnect the load as soon as the over-current event happening instead of waiting for the temperature goes high? Thanks.
Best regards,
Wayne