Other Parts Discussed in Thread: GPCCHEM
During testing of our battery board (cell configuration 4S2P) I found that the indicated battery capacity (RSOC/ASOC) drops over time when the board is on external power and the charger and/or the fets are disabled. When I than charge the set, it will not reach 100% charge level any more (because the cells are not discharged). Only after a full discharge of the pack I can reach 100% RSOC again.
I have included a log file of this case. The board is on external power, with fets and charger disabled with a full battery. The RSOC starts at 100% and drops with stes in 24 hours to 67%. The workaround is simple of course (don't disable the fets or the charger) but I wonder what causes this behavior. idle_mode.log