I'm using the LM5085 buck controller to create a 48V to 24V DC Buck Converter with a 8.8A Load
Thus far I have been able to get a 6A load to work but when the load is increased to 7A the transistor shorts out. The circuit went back to working with a 6A load when I replaced the transistor with a new one.
Here is the schematic:
Here's the board layout:
The transistor that is dying is SUD09P10-195-GE3
I know I need to work on shrinking the current loops but I don't believe that is the source of the current problem.
In case it is relevant, I have to switch to using MFA420PS48 (48V 8.8A) instead of a bench top power supply to test the 7A load.