This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24070: current sharing

Part Number: BQ24070

Hi,

I have an application where the battery limit is set at 600mA and the Load current is set at high (ILIM1).

ILIM1 high shows a max of 500mA.

If the load requires 1A, what happens?

a. if the input supply can support it, would this provide the 600mA to the battery plus the 1A to the load? (total 1.6A from the supply)

b.would it regulate the current from the source to a max of 500mA and the rest of the current would come from the battery (i.e. discharging the battery with a 500mA current)?

c.would it shut-off the path from the supply and all the current would be coming from the battery? (1A discharge from the battery)?

d. something else...

Thank you!

Best regards,

Alberto