Other Parts Discussed in Thread: LM3464A, LM5021, LM3464
Hello,
I've connected 4 LEDs to the 4 FETs and only 2 FETs can light up the LEDs. I did swap the LEDs to make sure that they are not the issue here. I don't know if this is an issue with the gate drive or the layout or the part itself. This is the second board that I purchased from you. The first board did not light up any LED from any FET. To the first board, I've added the 4.7K at the FET gate and still nothing. Let me know please if you can help with this issue. Thanks. Sana