Hi E2E,
We use TPS40322 2-Phase solution and find VFB will from 0.6V rising to 0.606V when heavy load.
We also use fan to cool down the IC , but no any improve.
Did you have any idea to fix this issue?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi E2E,
We use TPS40322 2-Phase solution and find VFB will from 0.6V rising to 0.606V when heavy load.
We also use fan to cool down the IC , but no any improve.
Did you have any idea to fix this issue?
Hi Qian,
Feedback resistor: RGND=9.31K ; Rtop=42.2k
No load :
VFB to AGND (Pin 4 to Pin 6) = 0.6V
Remote sense (Pin 11 to pin 10) = 3.327V
Heavy load (33A):
VFB to AGND (Pin 4 to Pin 6) = 0.606V
Remote sense (Pin 11 to pin 10) = 3.364V
We also change the Feedback resistor: RGND=2.2K ; Rtop=10k to avoid noise, but the no any improve.