This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: is there a replacement part with 2 thermistor inputs?

Part Number: BQ28Z610
Other Parts Discussed in Thread: BQ40Z50-R2, , BQ34Z100, BQSTUDIO, EV2400

Hello,

I have 2 questions.

1. The series resistor on the VC2 pin for cell balancing is 5 ohm. is there a valid range for this value? if i increase this value do i need to increase the value of resistor on VC1 as well?

2. This IC has just 1 thermistor input. since i am using 2 series cells, i will need to sense the cell temperature for each. is there a comparable part with 2 thermistor inputs or is there a way i can use the TS1 pin and connect 2 thermistors to it (though a mux for example)? 

Thanks,

Gaurav