In the TPS23753's datasheet, APD pin is described as "Pull APD above 1.5V to disable the internal PD hotswap switch". But, on my PCB board, if the pull-down resister is not 47kohm, the IC won't work. I want to know why.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the TPS23753's datasheet, APD pin is described as "Pull APD above 1.5V to disable the internal PD hotswap switch". But, on my PCB board, if the pull-down resister is not 47kohm, the IC won't work. I want to know why.
User5957374, You have submitted a question over the weekend so please give us until Monday morning, US time, to respond.
And, just to be clear, are you asking about the TPS23753 (not recommended for new designs) or TPS23753A?
Thank you for the post,
Hi User,
Do you have APD pulled down with a resistor because you want to disable the functionality of APD?
Per the datasheet, APD can be disabled with by connecting it to RTN. Have you tried with a 0 ohm resistor instead?