Hello Guys,
i am currently designing a custom 24V Lipo battery pack. I am planing to use a touch-button ic to enable the LED Display functionality.
The Touch IC which was selected is the AT42QT1011 from Microchip. This IC needs a power supply of 1.8V to 5.5V and about 80µA.
As i see in the evalboard you use the input voltage of cell 2 to power the "first" BQ771807 for the secondary overvoltage-protection.
Is this generally a good design practice? When i use cell balancing, the power of the touch IC, which is drawn from cell one would also result in discharging the other cells?
But i think the power draw from the touch IC is not really much and an additional LDO would also consume (probably more) power...
On which additional current draw it is better to use an additional switching regulator/LDO?
By the way: which GND net should i use for the device? VSS or the PGND net? I am not sure about this...
Another Question regarding the LEDCTNLA pin:
We use some additional LED´s to show some operating states. Is it possible to use the LEDCTNLA pin and connect it to the base of an NPN transistor which than switches the other LED´s on for the same amount of time as the SOC-LEDs are lighten up?
I am not quite sure about this., because as i see the LEDs are connected anti-parallel between the LEDCTNLx pins, so there musst be some switching/multiplexing going on?
LEDCTNLA is connected to LED1 on the evalboard, which should (for me) present the lowest possible SOC?
So could this implementation work?
Is it possible that one of your engineers could short check the schematics before layout design starts?
Kind Regards
Daniel