Part Number: BQ25890
Hello all,
Regarding the BQ25890 inductor value:
For some reason, there is no indication for the inductor's value selection (The PDF only contains information regarding the ripple current and saturation current)
The inductor value is showed only at the system example schematics, and there is no information regarding min/max values.
I need to know, if the inductor can be increased to 1.2uHy (due to the decrease in the value of inductance in high currents)
What is the maximum allowed value of the inductor?
Thanks
Nir