This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040: ISET & ISET2 setting

Part Number: BQ24040

hi,

this is a recurrent topic, probably due to the fact that BQ24040 has no power path and is a linear (input current = output current anyhow)...

the question is:

ISET2 = high, current limit @ 500mA regardless ISET (that can be used as current monitor)

ISET2 = flt, current limit @ 100mA, regardless ISET(that can be used as current monitor)

ISET2 = low, current limit programmed by ISET

is my understanding correct?

thanks a lot

KR

Vincenzo