Hi TI experts,
As title ,may I know what kind of load share IC support 54 Vout?
Currently, TPS2412 , UCC29002 or UCC39002 only work at 12Vout , thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Is there any reference schematic that can share with us?
CS+ & CS- connect to High side, and ADJ pin also connect to 54Vo
Question : How to connect them ( CS+ , CS- and ADJ that PIN max voltage is only 15V) ?
Note: SMPS that Vo is 54V
Thanks.
Hi HAN LEE,
CS+ & CS- voltage range is the input common mode range includes ground and the positive supply VDD, and there is a resister voltage divider for CS+ & CS- Pin.
VOUT doesn't connect to ADJ directly.The voltage at ADJ pin is VADJ = VOUT - RADJ * IADJ.
I have attached an user's guide of UCC39002, which introduces the component selection and design for the modules to be current shared. I think it can help you much on its use.sluu166a.pdf
Regards,
Teng