Other Parts Discussed in Thread: BQ25883,
Queries:
1. With no battery connected, input @ 5V:
Some input sources cause the SYS output to pulse on and off.
I thought it could be due to missing data lines but have tested some USB cables without D-/D+ lines which performed fine.
Specifically I have tested 3 adjustable bench power supplies with no current limit set (up to 4A capable) which, when connected to evaluation board @ 5V all cause this SYS pulsing.
Standard USB (PC/DCP) chargers have not shown this behaviour.
Is this the behaviour what FIGURE 25 of the device datasheet is demonstrating?
2. USB OnTheGo functionality/intelligence:
Is there any intelligence to how USB on the go is enabled/managed?
I know that it is enabled by pulling the OTG pin high BUT what happens if this happens when a charge source is already connected?
Does the device only output 5V if it detects there is not a charger present?
3. Do TI have any solutions to managing the audible noise generated when the device switches to PFM mode when under LOW load conditions?#
4. Are there any higher resolution images for the PCB artwork present in the evaluation board user guide (OR design files/gerbers)
These would be very useful for cross checking suggested layout guidelines from datasheet/user guide.