Other Parts Discussed in Thread: UCC28C40
Dear Sir,
I am making a flyback, the input voltage is 200VDC--800VDC, (150VDC~900VDC range will be better), output voltage is 13V, total output power is about 4W.
Can UCC28704 support this wide input voltage?
My original design is to use UCC28C40, transformer is EEL16, Npri=300,Naux=22, Lpri=8mH, it works well from 200V~800VDC input. But I need to reduce the power loss @light load. So I try to use UCC28704 with the same transformer, but it could not work normally, as the Voltage of Aux can not reach 13V, it can only reach <5V, it seems that the duty cycle has been limited, the power. I am not sure if the fault is due to transformer design or not, could you please help? If transformer problem, could you please advise the details? The WEBENCH tool doesn't support wide range input voltage.