This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61088: How to calculate passive component values for loop stability (at COMP pin) ?

Part Number: TPS61088

Hello,

I am using TPS61088 in an application. My application requirements are as shown below.  

Input voltage (V)

3 - 4.2

Output voltage (V)

6.6

Max Output Current (A)

1.5

I have few queries in selecting passive components for loop stability (at COMP pin). Please tell the values to be selected for GEA(Amplifier’s transconductance) and D (switching duty cycle) to calculate for passive components value.

Please find the datasheet link for your reference (http://www.ti.com/lit/ds/symlink/tps61088.pdf)

Regards.