Hello,
I have made an xls file to compute the charging compensation as describe in the app note #SLUA750
I do same computation for our 4 Cells battery. (xls file enclosed)BQ40z60 charging compensation calculation.xls
My result are :
set the data flash Voltage (cell based) to | 4052 |
set the voltage resolution to | 32 |
set the voltage register to | 245 |
Could you check and validate the change ?
Is this the only change to do ? (3 new values in data flash register)
Best regards
Gilles