Using a 12V 2A coupled inductor reference design, and at low output currents <400mA it runs well with no immediate side effects. Once we go over 400mA things change rapidly. At 1A it is getting very hot (cannot touch the coil) within approximately 30 seconds. If we try at 2A it is getting to a similar temperature in around 15 seconds. The output voltage appear OK, it just overheats and its mostly the coil. The Mosfet is heating up too, but the coil is most noticable.
Looking at the VSwitch waveforms at the different currents I can't help but feel they aren't right. The unit is running at the design frequency of 320KHz.
The above is with a 50mA load.
This is a 400mA Load.
Above is a 900mA Load
Finally a 2A load.
The loads are all resistive only, with only some lead inductance and capacitance.
Any hints? The coil tests OK for basic conductivity tests it is a Bourns catalogue product and unless the batch is faulty I have others with the same results.
Thanks in advance
Ken