This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: IDSELEN bit

Part Number: BQ27520-G4

I think two kind of cell profile is used when IDSELEN bit is 1.

In this case, should we confirm that Update Status 0 and 1 becomes "02"?

If it is yes, can we select cell profile which we want to update?

Best Regards,
Kohei Sasaki