This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28742: Why is the DRV source current so low? Will it lead to high swtiching loss ?

Part Number: UCC28742
Other Parts Discussed in Thread: UCC28C45,

 Customer is looking for a high efficiency aux solution(<30W),  and used UCC28C45 before. I recommend UCC28742 now, but they are confused that the DRV source current for UCC28742 is 30mA , while 1A for UCC28C45.  Will the swithing loss be very high for UCC28742 with such a low driving current for the high voltage mosfet?