Hi team,
My customer is using the UCC28881 to make a Fly-buck.
Here are the characteristics of this Fly-buck:
• Single-phase variable input voltage 85V rms - 265V rms
• Non isolated output (VOUT) 10V 10mA
• Isolated output (VAUX) 5V 300mA
The characteristics of the coupled inductors used for this Fly-buck cause a spike on the primary current at each closing of the internal MOSFET of the UCC28881.
The Fly-buck operates while this spike is over the I_LIM specified in the datasheet. They are assuming the spike have to be shorter than the blanking time of the UCC28881.
However, they would like to make sure that they have some margin for all operating points, However, there is nothing in the datasheet on the minimum duration of this blanking time. Would it be possible to have more information about it?
Thanks & Regards,
Pol