This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: chemical ID no match

Part Number: BQ34Z100-G1


Battery: single cell, 4.2V,  5000mAh

uploading the discharging log to TI webnet.but it  feedback no matched chemical ID.

Summary of all IDs with max. DOD deviation below 3%  
  
Chem ID max DOD error, % Max R deviation, ratio
0 0 0
  
Warning: Deviation is above recommended level. New chem ID needs to be released for this cell. Please contact your TI representative to send the cell to Dallas for characterization

chemical id 22-report.zip