This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1EVM: Output Channel have no Current

Part Number: LP8860-Q1EVM

Hello TI Team:

I got a problem about LED driver LP8860.

after power on, I set register table to be meet my setting. I also attached register table and schematic below.

After setting, I measure LED_Anode vs GND, it has 33V and match my setting in 0x73=22.

But I measure LED_Cathode1/2/3/4 vs GND, they are 0V. Then, I measure LED_Anode vs LED_Cathode 1/2/3/4, the result are 0V.

I'm confused that. I also check SQW output status and I think it should have square-waveform output but it is 0V. 

Could you help me to check what it is problem?

Bu the way, after power on and LED driver is enabled, if I don't connect LED light bar to these 4 channels. What status does the driver happen?

LP8860 Schematic_v9.2.pdf

LP8860 Register Setting.xlsx