HI Team
If the bottom pad of the LM43603-Q1 is not soldered properly, it is found that the output voltage is abnormal.
We have designed six vias in the bottom pad as shown in the datasheet.
However, in the SMT process, we found that lead leaked through the vias.
I would like to ask you some questions about this issue.
1. Why is the voltage unstable when the bottom pad is not properly soldered?
2. What percentage of the bottom pad area should be soldered for stable output?
3. What is the purpose of Vias in bottom pad? (Heat dissipation, GND strengthening, EMC enhancement, etc)
4. We are going to reduce Via of bottom pad from 6ea to 4ea.(System Spec : 12Vin -> 3.3Vout / 2A)
Is there any problem in reducing Via?
5. Is there a formula for calculating the number of vias required for a bottom pad?
If yes, please share it.
Thank you.