Part Number: TPS61193
Hello,
I am using a TPS61193 to turn on a 15-LED string, with a total Vf of 42V. The problem is the initial voltage (k=0.88), which is 40.59V with R1=910k and R2=130k, so the string sometimes does not start due to insufficient voltage and the component goes into error state.
I have two options:
1- raise R1 to 1Mohm: initial voltage will be 44,48, so the led string starts (tested), however the theoretical output voltage will be 49V, which will never be reached because the LED string will limit it.at 42V.
2- set R1 at 470k and R2 at 22k, thereforeobtaining initial voltage of 42,84 (tested and working) and maximum voltage at 45V (good). The thing is I am violating the recommendation to keep R2 at 130 kohm. Considering that I cannot modify the PCB because it has already been built (so a T-divider is not an option), what are the consequences of setting R2 at 22kohm?
Given the choice, what solution would you recommend in terms of reliability?
Thanks,
Paol.