Other Parts Discussed in Thread: TPS61099
Hi,
I'm using the TPS61220 to step up from a fixed 4.0V to 5.0V to supply USB devices. Everything works as expected, but if I disable the device (EN=0V) I still see a voltage at the output VOUT = 3.4V (when VIN = 4.0V). After digging into the datasheet I only can see the leakage current specified for Vout>Vin. So I guess we are using the the device in an unspecified manner. Is this correct? Is there any way to fix this?
Thanks and best regards
Stefan