Other Parts Discussed in Thread: TPS92515
Hello,
I have tried to connect PWM (after having set the right jumpers) and it damaged the board.
Any insights?
Thanks.
Sana
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have tried to connect PWM (after having set the right jumpers) and it damaged the board.
Any insights?
Thanks.
Sana
Hello Sana,
Did you remove R14?
"3.2.1.5 TP3, PWM
The PWM test point connects directly to the PWM pin of the TPS92515. Leave R14 connected for normal
operation. If PWM dimming is used, remove R14 and apply a square wave with a low level of GND and a
high level of between 2.5 V and 5 V. The dimming frequency range is 100 Hz to 10k Hz."
did you make sure the signal was below 5.5V and referenced correct?
Best Regards,
Hi Irwin,
Just a minor correction, I did not remove R14. I was not planning to carry on with teh EVM recommendations but because of the failure more, I've stopped.
Thanks.
Sana
Hello Sana,
R14 is a zero ohm resistor, PWM is shorted to VCC. It cannot dim this way. I am not sure what will happen if you drive PWM when it is shorted to VCC. It would depend on the impedance of the PWM source.
Best Regards,
Hi Irwin,
I did not remove R14 before connecting it to the PWM. That is what probably damaged the part. This resolves the issue. Thanks.
Sana