This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62745: Inquire TPS62745 Quiescent Current too high

Part Number: TPS62745


Hi Sir,

Please refer SCH as below, Vin=7.5V, Vo=3.3V, the Iin=5.5mA during no load, it's higher than datasheet quiescent current spec.

May I learn from you how we can improve quiescent current ?

Thank you.

Edward Chen

  • Hello user,

    The quiescent current is not a specification which could be improved by reworking the passive elements around the IC. Iq is defined as being the current drawn by the IC in a no-load and non-switching but enabled condition.

    Here is an app-note which explains really well the matter: http://www.ti.com/lit/an/slyt412/slyt412.pdf

    This ultra-low power area is a focus for Texas Instruments. We have new products fairly regularly. There is one device in particular which I think would be a great fit for your application, and it should be on the web and sampling here in a few weeks.

    If you can wait that long, great. If not, maybe you do a first board with the TPS62745 to start working on your system and switch to this new one on the next PCB spin.

    Thank you.

    Best Regards,

    Dorian

  • Hello user,

    I haven't heard back from you. 

    Do you have any further questions on the TPS62745? If you do, please reply below.

    Thank you very much!

    Best Regards,

    Dorian