Other Parts Discussed in Thread: BQ25101
Team,
PRE-TERM can be left floating so that the current is set to the default one given in the BQ25100 datasheet (SLUSBV8C page 6 - see below picture).
Those min/Typ/Max specs are given for Riset = 2.7kOhm.
-Is there any deviation in current when Riset is different?
-Do we have a curve showing the deviation/error for the Riset recommended range (Riset: 13.5 kΩ (10 mA) to 0.54 kΩ (250 mA))?
In this use case the battery is a 20mAh battery. Iout would be 11.25mA (ie using a 12kOhm Riset)) and the goal is to have 10% of Iout for TERM and 20% of Iout for PRE-CHARG.
-Any specific consideration for this scenario to have a closer look (like behavior at different temperature, Resistor tolerance, ..etc)?
Thanks in advance.
A.