Other Parts Discussed in Thread: BQ25713
The BQ25713 feature that when the ChargeCurrent Register (0x02~0x03) is all zeroes, VSys is regulated at whatever the battery voltage is plus 160mV. If such register is set to all zeroes at a point that the battery voltage is not at its fully-charged voltage state (e.g. perhaps a battery disconnection is needed because the battery is too hot), this will mean that VSys will be at a lower voltage than that specified at the ChargeVoltage Register (0x04~0x05) which would restrict the amount of available power at VSys.
Would the recommended practice then be to increase the MinimumSystemVoltage register (0x0c~0x0D) to a voltage close to (but less to) the ChargeVoltage Register when the ChargeCurrent Register is all 0 and reduce it to the normal lower voltage when not?