Hello,
I like to know what dimming resolution is actually achievable at output.
The input offers 16-bit. PWM is 13-bit best. Meaning, we would activate hybrid-dimming to achieve > 13 bit resolution. The current seems to be resolved with 12-bit according to datasheet.
It is not obvious, whether combination of 12-bit and 13-bit will achieve more than 13-bit. Is there something to consider like an optimal switch-point ?
I think with 12.5 % switch-point the ratio of maximum current vs. minimum average current is like a 16-bit LSB.
Thanks for your advice,
Martin