This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27402: Minimum on time

Part Number: LM27402


Hi all,

I have a customer who would like to use LM27402 to generate a 20V to 0.72V Buck Converter switching at 1MHz. I see a MAX duty cycle and minimum off time in the datasheet, but no minimum on time spec. 

Is it possible to use LM27402 in this application?

Thanks,

Jon

  • Hi,

    You are correct, i would be cautious operating this device at 1MHz. 

    When i tried using webench to ask me generating a design, the operating frequency is around 600kHz. 

    Do you know what is the load current that you are designing into? Maybe we can find another device that might be more suitable

    https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=975E81CFFB5E0DA8

    Thanks

    -Arief

  • Hi Arief,

    The datasheet says its capable of switching at 1MHz. Do you think this could just be an issue with the webench model?

    What is the minimum on time of this converter?

    If we were to use a different part, it would need to have frequency synchronization and be capable of switching at 1MHz.

    Thanks,

    Jon

  • Jon,

    Its 50ns: minimum on time

    If you have a low duty ration stick with the lowest operating frequency if possible.

    Regards,

    Mathew