Other Parts Discussed in Thread: BQ24650
Hi
I have a few more questions about the EVM schematic for the BQ24650.
1) Please tell me why the following components are included on the EVM Board for Part Number BQ24650 and also what purpose they perform. I have noticed that, with the exception of C15 - 22Pf they are not included on the data sheet schematic.
R11 - 100 Ohms, C17 - 22pf, C15 - 22pF, C1 - 10uF, C11- 0.1uF.
2) C13, C9 and R8 are designated as open (not populated). Are these NOT included due to a board EC or do they offer some sort option if require ? If so, can you explain?
3) I would have thought that R6 (sense resistor) would have been place after the output caps C7 and C8 and not before. Was there a reason for this – maybe not much of a difference?
4) Page 9, part 5 of the BQ24650 EVM guide refers to the "capacitors for the BAT". What capacitors are being refereed to here in the schematic on page 17.
5) From what I can tell, there is no reverse protection circuitry on the board or in the IC to protect against a battery being hooked up with reverse polarity. Is that correct?
Thanks
Dave