Hello TI,
I have designed a three phase inverter for operating current control to an 3-phase inductive load(2.2mH per phase). Operation is stable at 60V and upto 16A rms current. If i increase my input DC link voltage to 72V and at 6A rms current, output of the high side driver gets OFF for few pulses but input to the driver is proper. While debugging the circuit, i.e checking the bootstrap voltage( constant voltage 15V throughout i.e No issues) and the pulses at the input and output, the pulses from the controller to the driver (proper SPWM from control to the input to the driver), the state where high side output pulses went to the OFF state, there we could see that it somehow went little below then 0V.
I have attached the image during the OFF state of the high side pulse. Green pulses are the high side driver output pulses and Red pulses are the high side driver input pulses.
If the issues as suggested by application note of UCC27714 is the Undershoot voltage then for the same circuitry, i have increased my output gate resistance to 15ohms for initial 10ohms and also added schottky diodes to between HB and Ho and also between HO and Hs. But still the problem is resolved.
I have attached schematic as a reference for my driver circuitry with all the R and C parameters with their ratings.
As the output of the High side driver gets into OFF state, the output of my phase currents drops down.
I have attached output of phase current and in the attachment we can see that because of OFF state in high side driver the current in Blue phase drops down. And current in yellow phase and red phase in normal but it also gets hampered at voltage above 80V.