This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2662: Behavior between 0V < Vin <4.5V

Part Number: TPS2662

The behavior for negative input voltage is clearly defined. The same applies to an input voltage of 4.5V or higher.
Is there a defined behavior of the device in the range 0V < Vin < 4.5V (e.g. safely switched off)?
If an input voltage would change from the negative to the positive range, this range is passed through.
What happens then?

best regards,

Wilfried