This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24103A: Inductor Caclulation

Part Number: BQ24103A

How do we calculate the proper inductor value. The datasheet uses 30% inductor ripple current for the calculation.  Does the ripple current have a range or does it have to be 30%

  • Hi Bill,

    30%-40% is a generally accepted inductor current range for dc-dc converters.  If higher than that either the output voltage ripple gets too high for most applications or the current limit circuitry can no longer accurately measure the current.

    Regards,

    Jeff