This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A84A: accuracy for Iout less than 5mA

Part Number: TPS7A84A


The TPS7A84A datasheet specifies all output performance parameters (output voltage accuracy, line regulation, load regulation) from 5mA < Iout < 3A. Under Recommended operating conditions it lists output current as 0 to 3A. Is the output voltage accuracy only specified for > 5mA? If the load is less than 5mA is the accuracy worse than 1%?