Two questions:
1.BQT24157:When charging is disconnected, whether the output of VBUS will drop instantly
2.Seeking a charging management chip:
1)The battery can be powered by an external 5V input;
2)Regardless of whether the external input power supply ,It has a stable 5V output (current about 1A), there will be no short-term power-down phenomenon in the power path switching;
3) This 5V output can control the output by pressing the button short/long press.