Other Parts Discussed in Thread: EV2400, , BQ34Z100, BQSTUDIO
Hi all,
I'm current testing a BQ34Z100-G1 fuel gauge on an system side EMS. The device is connected to an STM32 MCU. For stand-alone testing and calibration I'm using the EV2400 and de-soldered series and pull-up resistors to the MCU.
So far I verified the +4V supply outputs a voltage around 3.5V and the VREG is able to regulate to 2.5V. I'm however unable to connect with the EV2400 connected to the I2C port (PORT 2). No ACK is received. I updated the EV2400 firmware to the latest 0.28 release.
I can tell that the EV2400 is sending data correctly, SI looks to be okay too after removing the clamping diodes. I measured at VEN and found that it pulses irregularly (>5s) with 120ms width indicating that it's sampling slowly. I can't find any stange behaviour on start-up either.
Is there any obvious mistakes I'm missing and is there a place to look next?
Thanks!
See attached schematic below: