Dear
I use BQ24170EVM-610-15V.Enter 12V on the J1 side,The output J2 VBAT and PGND are connected with 3 lithium batteries of 7.2V in parallel, and an ammeter is connected in series.
Then I want to set the charging current to 3.5A, modified R18=100K, R30=100K, and R32=27K
However, when I plugged in after the modification, the ammeter showed A current of only 2.4A and the LED light D1 was always on
Why is that?Is there anything else I need to change?