Other Parts Discussed in Thread: BQ40Z50EVM-561, , BQ24770EVM-540, BQSTUDIO, BQ24770
I am developing an NVDC battery system using the bq40z50-R2 gauge. My evaluation system is depicted in the attached diagram. I have confirmed that my bq24770EVM-540 is working correctly. But the bq40z50EVM-561 (containing the bq40z50-r2 gauge) is not.
I cannot get the bq40z50-r2 to allow for charging or discharging current to flow. I detach the communication bus plug (P2 in my diagram), set up the bq24770 charge controller using bqStudio to implement a charge current of 1216 mA, then I close bqStudio.
With the evaluation setup still powered, I plug P2 back in and restart bqStudio. The program instantly recognizes the bq40z50-r2 gauge and it appears to be communicating okay. But when I connect SYS PRES jumper to PACK- on the bq40z50EVM-561 (as described in the EVM user's guide to start the charge or discharge test), nothing happens.
I can't get any charge current to flow. Please let me know what steps to do to get my evaluation system working.
Thanks,
Carl Olen