Other Parts Discussed in Thread: LM3643, LM36010, LM3644
Hello,
I am considering using the TPS61500 for driving a couple of high power IR LEDs. I want to keep these LEDs on for 14 ms. As such, I am thinking of applying a 30 Hz PWM signal but as per the datasheet, the minimum recommended PWM frequency is 200 Hz. So, can I not use the TPS61500 as my LED driver? Also, if you have any other recommendations for keeping these LEDs on for 14 ms, that would be great. Thank you.
Sincerely,
Tajbid Rahman