Best solution for disable ic under 170v ac ?
Used pin vinac or used shutdown pin ?
Reference how can sure ic stop under voltage (170v)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Best solution for disable ic under 170v ac ?
Used pin vinac or used shutdown pin ?
Reference how can sure ic stop under voltage (170v)
Hello Omid,
The best way to disable the pwm is to used a comparator pulldown on the VSENSE pin.
So when the input is below 170Vac VSENSE is pulled below the open loop protection threshold of 0.75V
I do not have a reference design available to share with you but you will need to design so you will need to design the comparator circuit by yourself.
Regards
John