Other Parts Discussed in Thread: TPS61240, TPS62140
Hi team
I need to get a 3V to 12V programmable output voltage with 2A capability using TPS61240;
1, Why output voltage of TPS61240 is limited within 0.9V~6V?
2,I want to trim the FB pin to adjust the output voltage with following method, so I want to leave VOS unconnected, just use FB pin。Can I do this? If not, reason is?
many thanks!