Part Number: TPS54541
Hi
We are planning to apply TPS54541.
Is the over current protection function in the IC function?
Is it set to 5A standard or can it be set separately?
The second is 150 ° C TJ Operating Range. I want to know that THERMAL SHUTDOWN operates at 176 ° C.
Is it used at over 150 ° C? Does not the THERMAL SHUTDOWN operation protect the IC from operating below 150 ° C?