This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40090: Phase frequency set range

Part Number: TPS40090

HI Team,

I have a couple of questions

  1. I’m having a look at the implications of using the TPS40090. Please could you clarify the relationship between “Phase frequency set range … min 100 kHz, max 1200 kHz”, and “Synchronisation frequency range … min 800 kHz, max 9600 kHz”. I take it that “Phase frequency” is just what it says – the frequency in each output filter inductor. But “Synchronization frequency” is 8x that. I could guess that it’s twice the sum of the phase frequencies, but I’d appreciate some confirmation.
  2. DrMOS devices look like an obvious partner for the TPS40090, and I’ve looked at TI’s Power Stages. Are there parts with common pin outs with other manufacturers?