Use case is 24V Vout at 3A.
What is the minimum Vin required? For example, would it work at 26V Vin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eddie,
Usually there is a dropout voltage graph in the datasheet to help illustrate this. However since the LMZ14203H datasheet doesn't have this, I went ahead and took an EVM into the lab to test for dropout voltage. For 24V output at 3A loading, I noticed the output voltage dropped around 26.5V input. To air on the safe side, for 24V output at 3A loading, I would recommend the customer stay at 27V minimum.
Regards,
Jimmy