Other Parts Discussed in Thread: LM3404HV, TPS92512, TPS92513
Hi, how far can I push the LM3404HV? 60W? or is it set to 1A maximum. Can I run it at 1.4A constant current at 38V if I have good thermal management?
Best regards.
Marcos
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Marcos,
In the EC table:
ILIM Current Limit Threshold 1.2 1.5 1.8 A, so no, it is not recommended.
There are other parts that are capable of this, TPS92512, TPS92513, TPS92515A
Best Regards,