This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25085A: help check on the FB pin connection to GND

Part Number: LM25085A
Other Parts Discussed in Thread: LM5117

hi Team, 

my customer is evaluating the LM25085A for a constant current output design.

input: Battery pack voltage 17~29.4V

output voltage :Battery voltage

output current: continuous 7A, peak 15A 5 sec.

referring to the page 9 block diagram in the DS.

can we connect the FB pin to GND? so the voltage is not regulated and just limit the current?

any other effects if FB is connected to the GND? thanks