This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I plan to use 5 ADS7057 ADC simultaneously. I supply the AVDD rails using a REF2030 voltage reference with 20mA source current capability. The REF2030 maximum recommended output capacitor is 10uF. The ADS7057 datasheet recommend a 3.3uF decoupling capacitor on the AVDD rail. Is it fine if I put 1uF close to each ADC plus a 4.7uF on the output of the REF2030? Is there any better configuration? What is the recommended decoupling scheme?
Best regards,
Théo Meyer
Hi Theo,
The design scheme you are applying with using a 4.7uF on the REF2030 output and 5 1uF capacitors at the ADCs seems like the best solution for what you are trying to achieve and using common capacitor values. The additional recommendations I can make is make sure that you use low ESR ceramic caps to ensure a stable voltage.
Thanks,
Abhinav.